cancel
Showing results for 
Search instead for 
Did you mean: 

OV2640 camera CIF mode ??

zeros_and_ones1991
Associate III
Posted on October 09, 2015 at 22:56

Hullo guys, 

Im using the OV2640 sensor to stream video and everything worked fine when it is in the default UXGA mode. My images are 320*240 pixels, so I wanted to move to the CIF mode for faster frame rate . The problem is that the datasheet is a real mess and I'm not sure what I might be messing . I have the following registers with the corresponding values : 

{0x12, 0x10} // CIF mode 

{0x18, 0x43}

{0x19, 0x00}

{0x32, 0x09}

{0x03, 0x06}

{0xc0, 0x32}

{0xc1, 0x2A}

{0x50, 0x00}

{0x51, 0x64}

{0x52, 0x54}

{0x53,  0x00}

{0x54,  0x00}

{0x57,  0x00}

{0x5a,   0x50}

{0x5b,0x3c}

  {0x5c,  0x00}

//

// Those are the values that I changed from the previous working UXGA mode . 

Any ideas? 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 10, 2015 at 02:14

Perhaps there is an

OmniVision

leaning forum?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..