cancel
Showing results for 
Search instead for 
Did you mean: 

OTG_HS_FS doesn't work

guillaume
Associate
Posted on August 22, 2011 at 13:37

Hello,

I'm currently working on a STM32F207IG6. If we use the pins PA9, PA11 and PA12 there isn't any problem. But if we use the pins PB13, PB14 and PB15 configured has GPIO_AF_OTG_HS_FS, the usb doesn't even start (the pin PB15 (DP) doesn't even pull up).

Any idea why ?

#stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 22, 2011 at 15:48

Any idea why ?

From the information provided, one might guess the GPIOB clock is not enabled.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..