cancel
Showing results for 
Search instead for 
Did you mean: 

NVIC_EnableIRQ() causes Hardfault

klaas
Associate
Posted on November 05, 2013 at 19:34

Hello,

I'm using a STM32-discovery Board equiped with a STM32F100RB. Till now all I'm trying to do is to call the Interrupt-Handler of TIM3. But when calling NVIC_EnableIRQ(TIM2_IRQn) the programm is always running into the Hardfault_Handler.

Is there anybody who knows the reason for this behaviour?

thanks, Klaas.
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
frankmeyer9
Associate II
Posted on November 05, 2013 at 20:45

Till now all I'm trying to do is to call the Interrupt-Handler of TIM

3

. But when calling NVIC_EnableIRQ(TIM

2

_IRQn) the programm is always running into the Hardfault_Handler.

 

A typo ?

Check that you implemented the correct handler, and enabled the matching interrupt.

Posted on November 05, 2013 at 21:01

GNU/GCC typically dumps all unhandled interrupts in the same spot, via weak linkage.

With C++ watch for name mangling of the handler routines.

A Hard Fault could occur due to missing handler (naming or linkage), or the routine depending on variables/pointers you haven't properly initialized prior to enabling the interrupt.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Fristedt.Jan
Associate II
Posted on November 06, 2013 at 12:47

Here is a good article that helped me:

http://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.html

Slightly modified code:

/**

  * @brief  C part of hard fault handler

  * @brief  http://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.html

  * @param  pointer to stack frame

  * @retval none

  * @date   2013-10-07

  */

void irqGetStackFrame(uint32_t *stackframe)

{

  StackR0 = stackframe[0];

  StackR1 = stackframe[1];

  StackR2 = stackframe[2];

  StackR3 = stackframe[3];

  StackR12 = stackframe[4];

  StackLR = stackframe[5];

  StackPC = stackframe[6];

  StackPSR = stackframe[7];

  for(;;) {

  }

} /* irqGetStackFrame */

/**

  * @brief  assembler part of hard fault handler

  * @brief  http://www.freertos.org/Debugging-Hard-Faults-On-Cortex-M-Microcontrollers.html

  * @param  none

  * @retval none

  * @date   2013-10-07

  */

void HardFault_Handler(void)

{

  __asm volatile

    (

     '' tst lr, #4                    \n''

     '' ite eq                        \n''

     '' mrseq r0, msp                    \n''

     '' mrsne r0, psp                    \n''

     '' ldr r1, [r0, #24]                \n''

     '' ldr r2, handler2_address_const            \n''

     '' bx r2                        \n''

     '' handler2_address_const: .word irqGetStackFrame    \n''

    );

} /* HardFault_Handler */

Here is what I do with undefined interrupt handlers, the number passed to the default hanler helps to find the problem:

/**

  * @brief  default IRQ handler called by spurious interrupts

  * @param  irq: interrupt number

  * @retval none

  * @date   2013-10-04

  */

static void defaultIrqHandler(int irq)

{

  for (;;) {

  }

} /* defaultIrqHandler */

void NMI_Handler(void)

{

  defaultIrqHandler(-9);

}

void MemManage_Handler(void)

{

  defaultIrqHandler(-7);

}

void BusFault_Handler(void)

{

  defaultIrqHandler(-6);

}

void UsageFault_Handler(void)

{

  defaultIrqHandler(-5);

}

void SVC_Handler(void)

{

  defaultIrqHandler(-4);

}

void DebugMon_Handler(void)

{

  defaultIrqHandler(-3);

}

void PendSV_Handler(void)

{

  defaultIrqHandler(-2);

}

#if 0 //defined somewhere else

void SysTick_Handler(void)

{

  defaultIrqHandler(-1);

}

#endif

void WWDG_IRQHandler(void)

{

  defaultIrqHandler(0);

}

void PVD_IRQHandler(void)

{

  defaultIrqHandler(1);

}

void TAMP_STAMP_IRQHandler(void)

{

  defaultIrqHandler(2);

}

void RTC_WKUP_IRQHandler(void)

{

  defaultIrqHandler(3);

}

void FLASH_IRQHandler(void)

{

  defaultIrqHandler(4);

}

void RCC_IRQHandler(void)

{

  defaultIrqHandler(5);

}

etc...

klaas
Associate
Posted on November 07, 2013 at 09:09

Even if it's not the nicest solution I found one. I updated the CMSIS and Periph-Driver Package provided by ST from Version 3.3 to 3.4 and no it's working.

thanks for the replies anyway!
Posted on November 07, 2013 at 13:21

http://www.st.com/web/en/catalog/tools/PF257890

Perhaps it relates to broader support for different chips, different interrupt vectors/implementation based on part/pre-processor defines.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..