cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple devices on the same SPI bus but with different SPI configs

jean_prieur
Associate III
Posted on June 17, 2013 at 10:37

Hello,

I use the STM32F407 and I have to link 3 different slave devices on the same SPI bus (an accelerometer, a touchpad controller and a screen). I have no other solutions. Each device is activated with chip select pin (CS).

The problem is, devices have not the same SPI configuration, for example the accelerometer is driven by a clock at high level by default and the touchpad controller is driven by a clock at low level.

Does anyone has already used SPI with different configurations ? Can I change the SPI config each time I want to drive a device ?

Thanks for your advice !

Jean
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
jean_prieur
Associate III
Posted on June 18, 2013 at 11:59

It seems complicated to have something working well and fast. I think I need to change one of my device and make it I2C compatible. 

I was thinking SPI is a standard protocol and it's easy to link a lot of ICs but it's not !

Anyway thanks for your interesting solutions.

frankmeyer9
Associate II
Posted on June 18, 2013 at 13:20

It is hard for others to really estimate all requirements in context - so this is up to you.

You can build a prototype around some core functionality to prove your design, but this costs time, too.

Another idea - you could discard the internal DAC and use the GPIO pins for SPI instead.

There are plenty of serial DAC circuits around ...