cancel
Showing results for 
Search instead for 
Did you mean: 

Message Queue usage

Stepan Podhorsky
Associate II
Posted on May 25, 2017 at 15:47

Hello all,

I have problems with Message Queue in CMSIS-RTOS. I have following code

for putting C structures onto the Message Queue

BOOL

put_program_chunk(

main_controller_req_t

req){

main_controller_req_t

*p_req;

BOOL

retval;

BOOL

no_memory =

FALSE

;

osStatus

status;

uint8_t

tmp;

// allocate memory in pool

p_req = (

main_controller_req_t

*)osPoolAlloc(flash_pool);

#ifdef

APP_DEBUG

if

(p_req == NULL){

   printf(

'No more space in flash pool.\r\n'

);

}

#endif

if

(p_req != NULL){

*p_req = req;

// insert the prepared request into the transmission queue

// osOK = 0x0

if

(!osMutexWait(flash_queue_mutex, osWaitForever)){

   

// put the message into the queue

   

// wait 5

ms

?

   status = osMessagePut(flash_queue, (

uint32_t

)(p_req), 5);

   osMutexRelease(flash_queue_mutex);

   

if

(status ==

osOK

){

      tmp = 1;

   }

else

{

      tmp = 0;

   }

}

}

else

{

   no_memory =

TRUE

;

}

if

(no_memory){

   retval =

FALSE

;

}

else

{

   retval =

TRUE

;

}

return

retval;

}

As soon as I try to call the osMessagePut, the program stick somewhere in the osMessagePut

function and the function never returns any value. The Message queue is shared by two tasks.

One is a producer (with priority equal osPriorityLow

) and the second one is a consumer

(with priority equal osPriorityAboveNormal

). Producing task is processed each 100 ms and

consuming task each 20 ms. Can anybody give me any advice what I have been doing wrong?

Thanks in advance for any suggestions.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0