mbedtls server error on firefox
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-04-23 12:54 AM
Hi all.
I would like to use a SSL connection, so I tried the mbedtls server example found in
STM32Cube_FW_F7_V1.9.0\Projects\STM32F769I-Discovery\Applications\mbedTLS\SSL_Server
I used IAR_760 with no code optimization and Firefox 56.0 32bit as browser.
The discovery is connected directly to my PC, no DHCP, and fixed address 192.168.1.10 is set.
Before to start with SSL session I sent a ping to discovery to check the ethernet link. All OK.
When I start with the SSL connection
the answers on discovery display are:Waiting for a remote connection...... OK
Performing the SSL/TLS handshake ..... failed mbedtls_ssl_handshake returned -19056 (MBEDTLS_ERR_SSL_INVALID_MAC)Walking in the code I found the problem around these functions:
File ssl_tls.c
1567 static int ssl_decrypt_buf( mbedtls_ssl_context *ssl )
. . . /* * Decrypt and authenticate */ if( ( ret = mbedtls_cipher_auth_decrypt( &ssl->transform_in->cipher_ctx_dec, ssl->transform_in->iv_dec, ssl->transform_in->ivlen, add_data, 13, dec_msg, dec_msglen, dec_msg_result, &olen, dec_msg + dec_msglen, taglen ) ) != 0 ) { MBEDTLS_SSL_DEBUG_RET( 1, 'mbedtls_cipher_auth_decrypt', ret ); 1678 if( ret == MBEDTLS_ERR_CIPHER_AUTH_FAILED ) <------------------------ return( MBEDTLS_ERR_SSL_INVALID_MAC ); return( ret ); }Any suggestions?
Thank in advance