ldrex/strex/stm32f7
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-01-29 2:44 AM
Posted on January 29, 2017 at 11:44
Command Set exclusive recording / ldrex / strex reading. The program takes off on operations in the field of memory sram1 / 2 (stm32f746).
In cortex_m7 chip there are many options for internal memory (total 320 Kbytes), including:DTCM-RAM = 0x2000 0000 - 0x2001 0000SRAM1 = 0x2001 0000 - 0x2004 C000SRAM2 = 0x2004 C000 - 0x2050 0000All memory is in linear space. But ldrex / strex teams are working in the field of DTCM-RAM.My idea of an exclusive read / write operations: the shadow instruction register addresses ldrex / strex must be cleared by reading / writing to the given address of the cortex of the nucleus. Memory Operations in the cortex not the core should not cause an error exclusive read / write. ldrex / strex operations should have no impact outside the core cortex.But it turns out otherwise.Question - how to live with it, and what a treat.#ldrex-strex
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0