cancel
Showing results for 
Search instead for 
Did you mean: 

LCD TFT Hello World at 8bpp? How? on STM32429I DISCO

gustavo23
Associate II
Posted on March 22, 2015 at 02:49

Hi,

Using the STM32429I DISCO demo board which has a 320x240 TFT LCD.

Running one of the demos in the STM32CubeF4, that uses the ''STemWin'' library to write a ''Hello World!'' message on the LCD.

By default the demo uses the SRAM and it has a bit depth of 32bpp (bits per pixel).

Is it possible to change the code to only use 8bpp?

If I change the driver from:

#define DISPLAY_DRIVER_0   GUIDRV_LIN_32

to:

#define DISPLAY_DRIVER_0   GUIDRV_LIN_8

the project compiles, but the screen looks weird, and I can't see Hello World anymore. 

If I set it to:

#define DISPLAY_DRIVER_0   GUIDRV_LIN_16

I can kind see hello world 2 twice on the screen so there is some sort of width / height calculation issue, and not sure how to resolve it. Also I don't know if this is just a software thing, or if it would require a hardware change, like changing the lines going to the LCD?

I am new to development with an LCD so I am a bit lost. Any help appreciated.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0