cancel
Showing results for 
Search instead for 
Did you mean: 

lab manual for working with stm32f1xx

geoffreymbrown
Associate II
Posted on November 13, 2012 at 22:44

With help from this forum, I've developed a lab course using the STM32VL Discovery board over the past year.   A draft of the lab manual is available at

http://www.cs.indiana.edu/~geobrown/book.pdf

an overview of the course here  (sorry copyright materials are restricted)

http://cgi.cs.indiana.edu/~geobrown/c335

and the code templates used are here:

https://github.com/geoffreymbrown/STM32-Template

Feedback is welcome.

Geoffrey
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
jj2
Associate II
Posted on November 13, 2012 at 23:16

This is good news - thank you.   Will read/review over next few days.

Would you be so good as to detail how you chose that particular STM32F?  That - along with course content would be of much interest.

geoffreymbrown
Associate II
Posted on November 14, 2012 at 14:46

The decision had more to do with timing than anything else.  The development process started in Fall 2010 and the stm32vl discovery board had recently become available.  The later STM32L0 board doesn't seem very flexible.  The F3 and F4 boards are fabulous, but came too late to be considered.  We are working on a follow-on class which will use the F3 board.    My primary goal was to make everything off-the-shelf so students to could see a path to rolling their own projects.   Really, the only limitation of the VL discovery board is RAM (only 8K), but that hasn't been a big problem for teaching.  There are plenty of STM32F103 boards available which can use exactly the same source code.

Geoffrey

John F.
Senior
Posted on November 14, 2012 at 15:36

Geoffrey, this isn't a technical issue but I'm guessing that where you have ''Forward'' you meant ''Foreword''?

geoffreymbrown
Associate II
Posted on November 14, 2012 at 16:45

Yes indeed.   

Geoffrey