2016-09-09 3:59 AM
Hi,
I have updated CUBEMX version from 4.12 to 4.16. I create the MDK5 project using CubeMX...then I open it and it works. But when I attempt to manage Project items, I can't create a new GROUP (folder), Keil% doen't response and it gets stuck.
It was working flawless until I updated the CubeMX version this morning.Did it happen to anyone else, need to solve it??it is disgusting.
Also, is it possible to downgrade to 4.12 for example (was my previous installation)?Thanks in advance.
Regards
Carlos
2016-09-09 6:44 AM
Hi,
I checked this case and I have same issue using CubeMx 4.16.1 !It's not possible to downgrade previous version.Regards2016-09-12 11:20 PM
i had the same problem, i cound not move around files in the project-window.
workaround: