Skip to main content
sima
Associate III
March 8, 2009
Question

Jumping to Reset_Handler?

  • March 8, 2009
  • 2 replies
  • 937 views
Posted on March 08, 2009 at 19:29

Jumping to Reset_Handler?

    This topic has been closed for replies.

    2 replies

    sima
    simaAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hello again :D

    I'm compiling the QuickStart_STM32 exemple provided in Ride7 and looking at the generated memory map.

    If i start debugging and look at Memory View window the Reset Handler address looks like 0x0800 01E5.

    But in the Disassembly View window Reset_Handler has the address 0x0800 01E4.

    I have seen this on other examples too.

    What is going on, why does the address diff 1 byte address?

    (se picture)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hi sima,

    This behavior is correct and there is no issues there. In fact this is how Cortex-M3 is decoding the address and always the PC ( program counter) should have the LSB equal to 1, that means it is executing in Thumb2 state, if it moves accidentally to 0 , so in you case to xxxxxxE4 , it would create a INVSTATE fault because T bit is 0 (ARM state).

    for more details refer to

    http://infocenter.arm.com/help/topic/com.arm.doc.ddi0337e/DDI0337E_cortex_m3_r1p1_trm.pdf

    . Page 96/384 ( Note ) & Page 64/384 ( ''T'' bit definition )

    Cheers,

    STOne-32.

    [ This message was edited by: STOne-32 on 09-03-2009 00:06 ]