cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with PWM TIM3 on STM32F3Discovery board

andreaspiezia9
Associate III
Posted on January 17, 2014 at 18:31

Hi all,

I'd like to see a PWM with my oscilloscope, but I see nothing and I can't understand why. Can you help me? Thanks in advantage <I>

int main(void)
{
TIM_Config();
GPIO_Configuration();
/* Infinite loop */
while (1)
{
}
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOB clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_2); // TIM3 Channel1 PA6 AF2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // Or UP for open-collector sources
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
/********************************/
static void TIM_Config(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
__IO uint16_t CCR1_Val = 40961;
uint16_t PrescalerValue = 0;
/* TIM3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
/* ----------------------------------------------------------------------- */ 
TIM_DeInit(TIM3);
/* Compute the prescaler value we want TIM3 clk @8Mhz => Presc = 8*/
PrescalerValue = (uint16_t) ((SystemCoreClock) / 8000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 100;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Output Compare Timing Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* TIM3 enable counter */
TIM_Cmd(TIM3, ENABLE);
}

</I>
This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
andreaspiezia9
Associate III
Posted on January 17, 2014 at 18:32

BTW do you know how hlm format the code as code?

chen
Associate II
Posted on January 17, 2014 at 18:43

Hi

I think you want :

  /* Output Compare Timing Mode configuration: Channel1 */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

or the PWM2

Posted on January 17, 2014 at 19:09

You use the Paintbrush [<>] icon (top left)

Your problem here is that with a period of 100 you're never going to get the counter to reach 40961

Set

TIM_TimeBaseStructure.TIM_Period = 100-1; // Divide by 100

..

TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

TIM_OCInitStructure.TIM_Pulse = 50; // 100/2 is 50/50 duty

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andreaspiezia9
Associate III
Posted on January 18, 2014 at 14:22

Thank you but it doesn't work both with new period/pulse (100-1/50) and 

<> TIM_OCMode = TIM_OCMode_PWM1 </>

Any other idea?

Posted on January 18, 2014 at 15:23

Is PA6 clashing with the L3GD20 (SAO/SDO)?

Can't you use PA4 (TIM3_CH2)?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andreaspiezia9
Associate III
Posted on January 18, 2014 at 15:31

I'm just trying with TIM3_CH2 and let you know soon

andreaspiezia9
Associate III
Posted on January 18, 2014 at 15:42

Used TIM3_CH2 but it doesn't work, I reported the last code revision since I've lightly modified:

any ideas?

#include ''main.h''
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
uint16_t PrescalerValue = 0;
static void TIM_Config(void);
void GPIO_Configuration(void);
int main(void)
{
/* TIM Configuration */
TIM_Config();
GPIO_Configuration();
/* Compute the prescaler value */
PrescalerValue = (uint16_t) ((SystemCoreClock) / 1000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 100-1;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Output Compare Timing Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 50;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC2Init(TIM3, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* TIM3 enable counter */
TIM_Cmd(TIM3, ENABLE);
/* Infinite loop */
while (1)
{
}
}
static void TIM_Config(void)
{
/* TIM3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOB clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_2); // TIM3 Channel2 PA4 AF2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // Or UP for open-collector sources
GPIO_Init(GPIOD, &GPIO_InitStructure);
}

Posted on January 18, 2014 at 16:05

0690X00000605WzQAI.png
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andreaspiezia9
Associate III
Posted on January 18, 2014 at 19:41

Have you an example code for TIM stm32f3?