interrupt problem for dma in usart
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-03-09 8:58 AM
Posted on March 09, 2014 at 16:58
hi guys, i wanna use interrupt for dma that i set for USART2 Rx/Tx but i don't know how can i implement intrrupt functions , here is my code please tell me how can i use interrupt for Rx and Tx dma in my code:
#include ''stm32f4xx.h''void RCC_Configuration(void){ /* --------------------------- System Clocks Configuration -----------------*/ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);}void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /*-------------------------- GPIO Configuration ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);}void USART2_Configuration(void) USART_IniTypeDef USART_InitStructure; USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE);}uint8_t Rx_Buffer;void DMA_Rx_Configuration(void){ DMA_InitTypeDef DMA_InitStructure; DMA_DeInit(DMA1_Stream5); DMA_InitStructure.DMA_Channel = DMA_Channel_4; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; // receive DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&Rx_Buffer; DMA_InitStructure.DMA_BufferSize = (uint16_t)sizeof(Rx_Buffer); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA1_Stream5, &DMA_InitStructure); USART_DMACmd(USART2, USART_DMAReq_Rx, ENABLE); DMA_Cmd(DMA1_Stream5, ENABLE);}void init_LED(){ GPIO_InitTypeDef GPIO_InitStructure; /*-------------------------- GPIO Configuration ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOD, &GPIO_InitStructure);}uint8_t Tx_Buffer;void DMA_Tx_Configuration(){ DMA_InitTypeDef DMA_InitStructure; DMA_DeInit(DMA1_Stream6); DMA_InitStructure.DMA_Channel = DMA_Channel_4; DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral; // send DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&Tx_Buffer; DMA_InitStructure.DMA_BufferSize = (uint16_t)sizeof(Tx_Buffer); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA1_Stream6, &DMA_InitStructure); USART_DMACmd(USART2, USART_DMAReq_Tx, ENABLE); DMA_Cmd(DMA1_Stream6, ENABLE);}int main(){RCC_Configuration(); GPIO_Configuration(); USART2_Configuration(); DMA_Rx_Configuration(); DMA_Tx_Configuration(); init_LED(); uint8_t temp = 0; while(1){ temp = Rx_Buffer ; while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // USART_SendData(USART2, temp); Tx_Buffer = Rx_Buffer; if(temp > 0){ GPIO_SetBits(GPIOD,GPIO_Pin_12); GPIO_SetBits(GPIOD,GPIO_Pin_13); } }}
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-03-09 9:15 AM
Posted on March 09, 2014 at 17:15 DMA unit, channel, stream are impacted in a fashion described in RM0090
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..