2014-04-25 7:52 AM
Hi,
I'm using the F3 Discovery board as a Slave with hardware chip select. I have to communicate this board with another board using the PIC microcontroller acting as a Master. The problem is that the pin voltage of the master is 0-5v. And so i can't interface it directly with the F3 because of the non compatibility. I would know is someone knows a buffer circuit that permits to have 5v to 3v. I have to convert all the pins from 5v to 3v (MOSI,MISO,SCK, CSS)? Thanks in advance.2014-04-25 3:05 PM
Do a search on Level Shifter IC. The choice of part depends on what speed signals you are using.
Try SN74LVC4245A as a start.