cancel
Showing results for 
Search instead for 
Did you mean: 

independent watch dog in stm32l151c8t6

satya
Associate
Posted on August 03, 2013 at 13:12

we need activation of iwdg  active only in normal mode, deactive in stop mode.

satya.ch

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
bogusz
Associate II
Posted on June 02, 2015 at 10:58

Even in HAL drivers is written:

(+) Exit:

 

        (++) By issuing an interrupt or a wakeup event, the MSI RC oscillator is selected as system clock.

 

It's not true, because even IWDG will make a reset in this mode which is so bad and can't be avoided in any way.

Lynn Linse
Associate III
Posted on December 15, 2016 at 22:21

No, it can be avoided. Per the STM manuals there is something called the IWDG_STOP bit in the FLASH_OPTR register, which (if set) freezes the IWDG during stop. I'm actually digging through the forum looking for more explanation of what this means!