cancel
Showing results for 
Search instead for 
Did you mean: 

IAP and memory Jumping

Rahimi.Meysam
Associate II
Posted on May 25, 2015 at 20:52

hello

i am using an IAP program to load another program on stm32f4 device. the main program is an uCOS-II RTOS.

I have one problem:

at first there is no problem to go in to IAP program and then jump to main program. but when i return from main program to boot(IAP), at time that i want to return to main program, Hard Fault occurs.

the codes for jumping between programs is here:

JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4);

      Jump_To_Application = (pFunction) JumpAddress;

      /* Initialize user application's Stack Pointer */

      __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS);

      Jump_To_Application();

One Point that i realize during debug operation was that the first jump from IAP to main program(that is correct) has assign new value for SP by __set_MSP() but in the second jump(not correct) SP did not changed after __Set_MSP() .

I would be thank full for your guidance.

thank you.

#iap-stm32f4
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0