I2C Issues in STM32F215
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-06-26 3:50 AM
Posted on June 26, 2014 at 12:50
Hi,
I am using STM32F215(master) in my custom board. In this controller is connected to the MPU9150 sensor(slave) via I2C interface.I tried to read the slave Id of the slave device, but i am getting whatever i am sending the slave address.Here i note down one thing, after configured the i2c always i am getting the BUSY in SR2 register. I don't know the problem, please help me asap. Below is my configuration,read and write code for I2C. static void I2C_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; I2C_InitTypeDef I2C_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* GPIO Configuration */ /*Configure I2C SCL pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure); /*Configure I2C SDA pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Connect PXx to I2C_SCL */ // GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); /* Connect PXx to I2C_SDA */ // GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_I2C1); I2C_DeInit(I2C1); /*!< I2C Struct Initialize */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0xA0; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_ClockSpeed = I2C_SPEED; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_Init(I2C1, &I2C_InitStructure); I2C_Cmd(I2C1, ENABLE); // I2C_GenerateSTART(I2C1, ENABLE); } void MPU_Write(unsigned char Address,unsigned char DataVal) { I2C_GenerateSTART(I2C1, ENABLE); I2C_SendData(I2C1,MPU6050_SLAVE_WRT); I2C_SendData(I2C1,Address); I2C_SendData(I2C1,DataVal); I2C_GenerateSTOP(I2C1, ENABLE); } unsigned char MPU_Read(unsigned char Address) { int i; unsigned char c; I2C_GenerateSTART(I2C1, ENABLE); I2C_Send7bitAddress(I2C1, 0x68,I2C_Direction_Transmitter); I2C_SendData(I2C1,Address); I2C_Send7bitAddress(I2C1, 0x68,I2C_Direction_Receiver); //for(i=0;i<100000000;i++); c=I2C_ReceiveData(I2C1); I2C_GenerateSTOP(I2C1, ENABLE); return c; } Advance thanks for your help. Regards, Thirukkannan.P
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0