cancel
Showing results for 
Search instead for 
Did you mean: 

I2C EEPROM Read with DMA

stst9183
Associate II
Posted on April 30, 2010 at 12:03

I2C EEPROM Read with DMA

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
stst9183
Associate II
Posted on May 17, 2011 at 13:49

With own risk!!!!

void fram_write(uint16_t address, uint8_t* buffer, uint32_t length)

{  

  DMA_InitTypeDef    DMA_InitStructure;

  if(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY) == SET)

  {

       i2c_bus_reset();

  }

    /* Care! Other FRAM Memory Sizes use different addressing (1 byte or 2 byte etc.)*/

    //((((uint8_t*) &address)[2] << 1) | I2C2_SLAVE_ADDRESS7);

    fram_slave_Address = I2C2_SLAVE_ADDRESS7;

    fram_RW_DataBuffer[0] = ((uint8_t*) &address)[1];

    fram_RW_DataBuffer[1] = ((uint8_t*) &address)[0];

   

    if(length > 0)

    {

        /* The first 2 bytes are address bytes msb first */

        memcpy(&fram_RW_DataBuffer[2], buffer, length);

    }

    iic_direction = IIC_DIRECTION_TRANSMITTER;

    I2C_AcknowledgeConfig(I2C1, DISABLE);

   

    DMA_DeInit(DMA1_Channel6);

    DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)I2C1_DR_Address;

    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST;

    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_MemoryDataSize_Byte;

    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

    DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;

    DMA_InitStructure.DMA_Priority =  DMA_Priority_VeryHigh;

    DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

    DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)fram_RW_DataBuffer;

    DMA_InitStructure.DMA_BufferSize = length + 2;

    DMA_Init(DMA1_Channel6, &DMA_InitStructure);

    I2C_DMACmd(I2C1, ENABLE);

    DMA_ITConfig(DMA1_Channel6, DMA_IT_TC, ENABLE);

   

    I2C_ITConfig(I2C1, I2C_IT_EVT, ENABLE);

    I2C_GenerateSTART(I2C1, ENABLE);

    fram_wait_ready();

}

void fram_read(uint16_t address, uint8_t* buffer, uint32_t length)

{

    DMA_InitTypeDef    DMA_InitStructure;

    fram_write(address, NULL, 0);

    iic_direction = IIC_DIRECTION_RECEIVER;

    DMA_DeInit(DMA1_Channel7);

    DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)I2C1_DR_Address;

    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_MemoryDataSize_Byte;

    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

    DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;

    DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;

    DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

    DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)fram_RW_DataBuffer;

    DMA_InitStructure.DMA_BufferSize = length;

    DMA_Init(DMA1_Channel7, &DMA_InitStructure);

    I2C_ITConfig(I2C1, I2C_IT_EVT, ENABLE);

    /* Set Last bit to have a NACK on the last received byte */

    I2C_DMALastTransferCmd(I2C1, ENABLE);

    I2C_DMACmd(I2C1, ENABLE);

    /* Enable the DMA Channel7 Transfer Complete IT */

    DMA_ITConfig(DMA1_Channel7, DMA_IT_TC, ENABLE);

    I2C_AcknowledgeConfig(I2C1, ENABLE);

    /* Generate the START */

    I2C_GenerateSTART(I2C1, ENABLE);

    fram_wait_ready();

    memcpy(buffer, fram_RW_DataBuffer, length);

 

}

Singh.Harjit
Senior II
Posted on May 17, 2011 at 13:49

Joachim, the I2C documentation says that DMA only works for receiving 2 bytes or more.

So, it looks like the code you have won't work for one byte. What do you do if you want to read only one byte?