cancel
Showing results for 
Search instead for 
Did you mean: 

i can't get work accelerometer

Dudenkov.Vladimir
Associate II
Posted on March 17, 2017 at 10:14

Lis2dh connect with stm32l151 on i2c bus.

function initial i2c:

I2C_DeInit( I2C1 );

RCC_APB1PeriphClockCmd( RCC_APB1Periph_I2C1, ENABLE );

RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOB, ENABLE );

GPIO_PinAFConfig( GPIOB, GPIO_PinSource9, GPIO_AF_I2C1 );

GPIO_PinAFConfig( GPIOB, GPIO_PinSource8, GPIO_AF_I2C1 );

GPIO_InitTypeDef accelerometer_gpio;

accelerometer_gpio.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;

accelerometer_gpio.GPIO_Mode = GPIO_Mode_AF;

accelerometer_gpio.GPIO_Speed = GPIO_Speed_40MHz;

accelerometer_gpio.GPIO_OType = GPIO_OType_OD;

accelerometer_gpio.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_Init( GPIOB, &accelerometer_gpio );

I2C_InitTypeDef accelerometer_i2c;

accelerometer_i2c.I2C_Ack = I2C_Ack_Enable;

accelerometer_i2c.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

accelerometer_i2c.I2C_ClockSpeed = 100000;

accelerometer_i2c.I2C_DutyCycle = I2C_DutyCycle_2;

accelerometer_i2c.I2C_Mode = I2C_Mode_I2C;

accelerometer_i2c.I2C_OwnAddress1 = 0x15;

I2C_Init( I2C1, &accelerometer_i2c );

I2C_Cmd( I2C1, ENABLE );

And then i trying send SAD+W command on accelerometer (in description he have 0x30-0x33 adresses):

while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));

I2C_GenerateSTART(I2C1, ENABLE);

while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

I2C_Send7bitAddress(I2C1, 0x25 << 1, I2C_Direction_Transmitter);

while (! I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); << this line!!!

I2C_SendData(I2C1, 0x20);

while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

but on 5 line program is hanging.

may be i do smth wrong?

#stm32l151 #lis2dh
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Francesco Murru
Associate II
Posted on September 21, 2017 at 23:52

Hi,

See my question, and, maybe, a solution: 

https://community.st.com/0D50X00009XkYN7SAN

 

Regards,

Francesco