cancel
Showing results for 
Search instead for 
Did you mean: 

I²S on STM32F411

florent2
Associate II
Posted on June 30, 2015 at 15:49

Hi!

I'm trying to communicate with a

http://www.cirrus.com/en/pubs/proDatasheet/CS4344-45-48_F2.pdf

DAC via I²S but I can't get it to work. I followed the steps on the STM32's HAL

http://www.st.com/st-web-ui/static/active/jp/resource/technical/document/user_manual/DM001058pdf#page=419

but I guess I made one or several mistakes as I don't get any output on any of the I²S pins. Here is my code :


#include ''mbed.h''


I2S_InitTypeDef CS4344_conf;

I2S_HandleTypeDef CS4344;

GPIO_InitTypeDef SDIN;

GPIO_InitTypeDef SCLK;

GPIO_InitTypeDef LRCLK;

GPIO_InitTypeDef MCLK;

uint16_t buf[2] = {0x1245, 0x6842};


int
main() {

CS4344_conf.Mode = I2S_MODE_MASTER_TX;

CS4344_conf.Standard = I2S_STANDARD_PHILIPS;

CS4344_conf.DataFormat = I2S_DATAFORMAT_16B;

CS4344_conf.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;

CS4344_conf.AudioFreq = I2S_AUDIOFREQ_96K;

CS4344_conf.CPOL = I2S_CPOL_LOW;

CS4344_conf.ClockSource = I2S_CLOCK_PLL;

CS4344_conf.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;


CS4Instance = SPI3;

CS4Init = CS4344_conf;


HAL_I2S_MspInit (&CS4344);


//-------- Enable the SPIx interface clock. 

__HAL_RCC_SPI3_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

__HAL_I2S_ENABLE(&CS4344);


//-------- I2S pins configuration: 

SDIN.Pin = GPIO_PIN_5;

SDIN.Mode = GPIO_MODE_AF_PP;

SDIN.Pull = GPIO_PULLUP;

SDIN.Alternate = GPIO_AF6_SPI3;


SCLK.Pin = GPIO_PIN_3;

SCLK.Mode = GPIO_MODE_AF_PP;

SCLK.Pull = GPIO_PULLUP;

SCLK.Alternate = GPIO_AF6_SPI3;


LRCLK.Pin = GPIO_PIN_15;

LRCLK.Mode = GPIO_MODE_AF_PP;

LRCLK.Pull = GPIO_PULLUP;

LRCLK.Alternate = GPIO_AF6_SPI3;


MCLK.Pin = GPIO_PIN_10;

MCLK.Mode = GPIO_MODE_AF_PP;

MCLK.Pull = GPIO_PULLUP;

MCLK.Alternate = GPIO_AF6_SPI3;


HAL_GPIO_Init (GPIOB, &SDIN);

HAL_GPIO_Init (GPIOB, &SCLK);

HAL_GPIO_Init (GPIOB, &MCLK);

HAL_GPIO_Init (GPIOA, &LRCLK);


// ------------- Program the Mode, Standard, Data Format, MCLK Output, Audio frequency and Polarity using HAL_I2S_Init() function.

//HAL_I2S_MspInit (&CS4344);


HAL_I2S_Init (&CS4344);


while
(1) {

HAL_I2S_Transmit (&CS4344, buf, 2, 1000);


}

}

What am I doing wrong? all the other example codes on the internet are using a different HAL (the functions don't match to the ones in the reference...)
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
florent2
Associate II
Posted on June 30, 2015 at 16:42

I also made a second code using bits of things I found online :


#include ''mbed.h''

#define M_PI 3,1415926535897932384626433832795

const
uint16_t wt01[255] = { 2047, 2097, 2147, 2198, 2248, 2298, 2348, 2398, 2447, 2497, 2546, 2595, 2643, 2691, 2739, 2786, 2833, 2879, 2925, 2970, 3015, \

3059, 3103, 3145, 3188, 3229, 3270, 3310, 3349, 3388, 3426, 3462, 3498, 3534, 3568, 3601, 3633, 3665, 3695, 3725, 3753, 3780, \

3807, 3832, 3856, 3879, 3901, 3922, 3941, 3960, 3977, 3993, 4008, 4022, 4035, 4046, 4056, 4065, 4073, 4079, 4085, 4089, 4092, \

4093, 4093, 4093, 4090, 4087, 4082, 4076, 4069, 4061, 4051, 4041, 4029, 4015, 4001, 3985, 3969, 3951, 3932, 3911, 3890, 3868, \

3844, 3819, 3793, 3767, 3739, 3710, 3680, 3649, 3617, 3584, 3551, 3516, 3481, 3444, 3407, 3369, 3330, 3290, 3250, 3209, 3167, \

3124, 3081, 3037, 2993, 2948, 2902, 2856, 2809, 2762, 2715, 2667, 2619, 2570, 2521, 2472, 2423, 2373, 2323, 2273, 2223, 2173, \

2122, 2072, 2021, 1971, 1920, 1870, 1820, 1770, 1720, 1670, 1621, 1572, 1523, 1474, 1426, 1378, 1331, 1284, 1237, 1191, 1145, \

1100, 1056, 1012, 969, 926, 884, 843, 803, 763, 724, 686, 649, 612, 577, 542, 509, 476, 444, 413, 383, 354, 326, 300, 274, 249, \

225, 203, 182, 161, 142, 124, 108, 92, 78, 64, 52, 42, 32, 24, 17, 11, 6, 3, 0, 0, 0, 1, 4, 8, 14, 20, 28, 37, 47, 58, 71, 85, \

100, 116, 133, 152, 171, 192, 214, 237, 261, 286, 313, 340, 368, 398, 428, 460, 492, 525, 559, 595, 631, 667, 705, 744, 783, \

823, 864, 905, 948, 990, 1034, 1078, 1123, 1168, 1214, 1260, 1307, 1354, 1402, 1450, 1498, 1547, 1596, 1646, 1695, 1745, 1795, \

1845, 1895, 1946, 1996 };


I2S_HandleTypeDef hi2s2;

/* I2S2 init function */

void
MX_GPIO_Init(
void
) {

GPIO_InitTypeDef GPIO_InitStruct;


/* GPIO Ports Clock Enable */

__GPIOH_CLK_ENABLE();

__GPIOC_CLK_ENABLE();

__GPIOB_CLK_ENABLE();

__GPIOA_CLK_ENABLE();


/*Configure GPIO pin : PC9 */

GPIO_InitStruct.Pin = GPIO_PIN_9;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

}

static
void
SystemClock_Config(
void
)

{

RCC_ClkInitTypeDef RCC_ClkInitStruct;

RCC_OscInitTypeDef RCC_OscInitStruct;


RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLM = 8;

RCC_OscInitStruct.PLL.PLLN = 336;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

RCC_OscInitStruct.PLL.PLLQ = 4;

HAL_RCC_OscConfig(&RCC_OscInitStruct);


RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);


}

void
MX_I2S2_Init(
void
)

{


hi2s2.Instance = SPI2;

hi2s2.Init.Mode = I2S_MODE_MASTER_RX;

hi2s2.Init.Standard = I2S_STANDARD_PHILLIPS;

hi2s2.Init.DataFormat = I2S_DATAFORMAT_16B;

hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;

hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_44K;

hi2s2.Init.CPOL = I2S_CPOL_LOW;

hi2s2.Init.ClockSource = I2S_CLOCK_PLL;

hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;

HAL_I2S_Init(&hi2s2);


}


void
HAL_I2S_MspInit(I2S_HandleTypeDef* hi2s)

{


GPIO_InitTypeDef GPIO_InitStruct;

if
(hi2s->Instance==SPI2)

{

/* Peripheral clock enable */

__SPI2_CLK_ENABLE();


/**I2S2 GPIO Configuration 

PC2 ------> I2S2_ext_SD

PC3 ------> I2S2_SD

PA6 ------> I2S2_MCK

PB10 ------> I2S2_CK

PB12 ------> I2S2_WS

*/

GPIO_InitStruct.Pin = GPIO_PIN_2;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF6_I2S2ext;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);


GPIO_InitStruct.Pin = GPIO_PIN_3;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);


GPIO_InitStruct.Pin = GPIO_PIN_6;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF6_SPI2;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);


GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_12;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

}

}

/* USER CODE BEGIN 0 */

#define BufferSize 255

uint16_t InputBuffer[BufferSize];

uint16_t OutputBuffer[BufferSize];

/* USER CODE END 0 */


int
main(
void
)

{


/* USER CODE BEGIN 1 */


/* USER CODE END 1 */


/* MCU Configuration----------------------------------------------------------*/


/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();


/* Configure the system clock */

SystemClock_Config();


/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_I2S2_Init();


/* USER CODE BEGIN 2 */

uint16_t i;

for
(i=0;i<BufferSize;i++)

{

InputBuffer[i]=0xFFFF;

}

for
(i=0;i<BufferSize;i++){

OutputBuffer[i]=wt01[i];

}

// HAL_I2S_Receive_DMA(&hi2s2, InputBuffer, 20000);

while
(__HAL_I2S_GET_FLAG(&hi2s2, I2S_FLAG_TXE) != 1);

HAL_I2SEx_TransmitReceive(&hi2s2, OutputBuffer, InputBuffer, BufferSize, 1000);

/* USER CODE END 2 */


/* Infinite loop */

/* USER CODE BEGIN WHILE */

while
(1)

{

/* USER CODE END WHILE */


/* USER CODE BEGIN 3 */

while
(__HAL_I2S_GET_FLAG(&hi2s2, I2S_FLAG_TXE) != 1);

for
(i=0;i<BufferSize;i++)

{

OutputBuffer[i]=InputBuffer[i];

}

HAL_I2SEx_TransmitReceive(&hi2s2, OutputBuffer, InputBuffer, BufferSize , 1000);


}

/* USER CODE END 3 */


}

But it's not working either...