cancel
Showing results for 
Search instead for 
Did you mean: 

HSE code generation not working

pnunes
Associate
Posted on May 28, 2015 at 12:13

Using STM32CubeMX to generate code for STM32F427ZITx processor. When changing the clock source from HSI to HSE the generated code updates the PLL fields but still maintains the source of the clock as HSI as shown below.

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 16;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

  RCC_OscInitStruct.PLL.PLLM = 8;

  RCC_OscInitStruct.PLL.PLLN = 336;

  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

  RCC_OscInitStruct.PLL.PLLQ = 7;

  HAL_RCC_OscConfig(&RCC_OscInitStruct);

I'm assuming this is a bug in the tool. Is there a fix? I have rewritten the code by hand but it would be awesome if this got fixed in the tool.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0