cancel
Showing results for 
Search instead for 
Did you mean: 

How to remap PD0/PD1 for STM32101C8 ?

anran99
Associate II
Posted on May 26, 2008 at 17:34

How to remap PD0/PD1 for STM32101C8 ?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
anran99
Associate II
Posted on May 17, 2011 at 12:35

Pls give a correct example, I can't post my code.

[ This message was edited by: anran99 on 14-05-2008 07:07 ]

julien
Associate II
Posted on May 17, 2011 at 12:35

I suppose that you want to remap the CAN on the GPIO D0/D1

//CAN Remappper sur D0 et D1

GPIO_PinRemapConfig(GPIO_Remap2_CAN, ENABLE);

/* Configure CAN pin: RX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOD, &GPIO_InitStructure);

/* Configure CAN pin: TX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(GPIOD, &GPIO_InitStructure);

[ This message was edited by: julien.massot on 14-05-2008 14:28 ]

anran99
Associate II
Posted on May 17, 2011 at 12:35

thx, but It's STM32101C8 . PD0/PD1 remap on OSC_IN and OSC_OUT pin.

I can't set the PD0/PD1 as output mode !

Maybe this is a bug ,I couldn't resolved it .

I need a demo sourcecode to remap .

appreciate your help .:D

anran99
Associate II
Posted on May 17, 2011 at 12:35

my test code :

/**********************************************************************/

void RCC_Configuration(void)

{

/* RCC system reset(for debug purpose) */

RCC_DeInit();

/* Enable Prefetch Buffer */

FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

/* Flash 2 wait state */

FLASH_SetLatency(FLASH_Latency_2);

/* HCLK = SYSCLK */

RCC_HCLKConfig(RCC_SYSCLK_Div1);

/* PCLK2 = HCLK */

RCC_PCLK2Config(RCC_HCLK_Div1);

/* PCLK1 = HCLK/2 */

RCC_PCLK1Config(RCC_HCLK_Div2);

/* PLLCLK = 8MHz * 9 = 72 MHz */

RCC_PLLConfig(RCC_PLLSource_HSI_Div2, RCC_PLLMul_12);

/* Enable PLL */

RCC_PLLCmd(ENABLE);

/* Wait till PLL is ready */

while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

{

}

/* Select PLL as system clock source */

RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

/* Wait till PLL is used as system clock source */

while(RCC_GetSYSCLKSource() != 0x08)

{

}

}

}

int main()

{

/* Configure the system clocks */

RCC_Configuration();

/* NVIC Configuration */

NVIC_Configuration();

/* Enable SWJ , Disable JTAG */

GPIO_PinRemapConfig( GPIO_Remap_SWJ_JTAGDisable , ENABLE );

/* AFIO Periperal Clock Enable */

RCC_APB2PeriphClockCmd( RCC_APB2Periph_AFIO,ENABLE );

/* Enable GPIO clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE);

GPIO_PinRemapConfig( GPIO_Remap_PD01 , ENABLE );

/* Configure PD.0, PD.1 as Output push-pull */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 ;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(GPIOD, &GPIO_InitStructure);

// while (1)

// {

// GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// GPIO_SetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// GPIO_ResetBits(GPIOD, GPIO_Pin_0 | GPIO_Pin_1 );

// }

}

jj
Associate II
Posted on May 17, 2011 at 12:35

Hi - am awaiting new board run - perhaps this suggestion may help:

Can't find obvious error in your listing. Would like you to move this

code to two other ''shared pins'' - and see IF the inability to set as

output persists. In this manner you - at least - will see if the problem is PD0/PD1 specific. Again - you must comb your part's pin-outs to find suitable (those which aren't ''natually'' I/O) pins to ''re-map.''

16-32micros
Associate III
Posted on May 17, 2011 at 12:35

Hi,

Check our last documents on web RM0008 version 4 and Erratasheet version 3 ( May 2008) Let me know if you get more questions on this.

Cheers,

STOne-32.