Question
How to implement SMBus v2.0 in STM32F4?
Posted on June 08, 2017 at 11:09
I found the library x-cube-smbus, but it is support only the STM32F0 and STM32F3.
And in the example in the file readme.txt it is written that:
'- This example has been tested with STM32F3-Discovery boards and can be easily tailored to any other supported device and development board.'In the datasheet on STM32F4, it is also said that I2C supports the protocol SMBus v2.0. I still have not seen a single example or a hint that this library is implemented in STM32F4.
I ask anyone who has information on this question to answer:
How things really are? Is it possible to do this?