cancel
Showing results for 
Search instead for 
Did you mean: 

How to erase the chip?

11andrey54
Associate
Posted on May 24, 2012 at 16:36

I use ST Visual Programmer and

http://www.st.com/internet/evalboard/product/250863.jsp

. During programming I set Read Protection ON. But now I can not erase or reprogramming the chip (STM32F103RB). I can see ''The device is protected'' only. How can I do this?
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dhutchison1945
Associate II
Posted on May 25, 2012 at 09:40

you have to disable the read out protection before

regards

spectre

frankmeyer9
Associate II
Posted on May 25, 2012 at 10:09

I did not yet mess with Visulal Programmer, but a ''Full Erase'' should be possible anyway.

The CRP feature is described in detail in the stm32f10x reference manual. I would avoid it if possible...

11andrey54
Associate
Posted on May 25, 2012 at 14:55

 

Yes, I have to disable the read out protection before. But I should be able to erase the chip in the future. And I can't do it via ST Visual Programmer. What are opinions?

 

Posted on May 25, 2012 at 16:23

What are opinions?

 

Serial port, or JTAG

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/CAN Bootloader. Commands with ROP dependece&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=446]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FCAN%20Bootloader.%20Commands%20with%20ROP%20dependece&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=446

I've also done it with code I built into one of my applications.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..