cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect micro sd using SDIO in 1 bit bus mode?

fb2
Associate II
Posted on December 12, 2014 at 17:50

I'm drawing a new pcb, and I cant find information on what to do with the other datalines not used... anyone can help me please? Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on December 12, 2014 at 18:30

I'd imagine you could just pull them high with a 33K or 47K, I certainly wouldn't leave them floating. This is really something you need to do your own due diligence on, shouldn't be that hard not to configure the pins in question, and verify operation.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
fb2
Associate II
Posted on December 12, 2014 at 18:46

Thank you for your reply Clive1.

Indeed, it is easy to do that test, but what I want to know is what is the correct (not only ''a way that works'') way to leave this pins... I imagine pulled up, but maybe something else too.

Regards and thank you again.