cancel
Showing results for 
Search instead for 
Did you mean: 

How to config STM32CubeMX 4.8.0, to make this PWM config Code ?

wjandsq
Associate III
Posted on June 14, 2015 at 14:13

uint32_t SystemCoreClock = 168000000;

uint32_t TIM4_PWM_frequency;

uint16_t TIM4_CCR1_SRC[1024];

uint16_t DMA1_TIM4_Pulse_Number = 10;

/**

  * @brief  Configure the TIM4 CH1 as PWM out.

  * @param  None

  * @retval None

  * made by wjandsq@163.com

  */

void TIM4_PWM_DMA_Config(void)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  DMA_InitTypeDef DMA_InitStructure;

  NVIC_InitTypeDef NVIC_InitStructure;

  TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

  TIM_OCInitTypeDef  TIM_OCInitStructure;

  uint16_t uhTimerPeriod = 0;

  uint16_t i;

  

  TIM4_PWM_frequency = 500000; // 500KHz

  uhTimerPeriod = (uint16_t) ((SystemCoreClock /2) / TIM4_PWM_frequency) - 1;

  TIM4_CCR1_SRC[0] = uhTimerPeriod / 2;

  

  for(i = 1; i < 1024; ++i){

    TIM4_CCR1_SRC[i] = TIM4_CCR1_SRC[0];

  }  

  

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);

&sharpifdef USE_PB6_PWM

  // TIM4_CH1_PWM: USE_PB6

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);

  

  /* GPIOB Configuration: TIM4 CH1 (PB6) */

  GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6;

  GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_DOWN;

  GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* Connect TIM4 pins to AF2 */  

  GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_TIM4);

&sharpelse

  // TIM4_CH1_PWM: USE_PD12

  /** TIM4 GPIO Configuration

    PD12 ------> TIM4_CH1

    PD13 ------> TIM4_CH2

    PD14 ------> TIM4_CH3

    PD15 ------> TIM4_CH4

  */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

  

  /* GPIOB Configuration: TIM4 CH1 (PD12) */

  GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12;

  GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_DOWN;

  GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_Init(GPIOD, &GPIO_InitStruct);

  /* Configure GPIO pin alternate function */

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);

&sharpendif

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1 , ENABLE);

  DMA_DeInit(DMA1_Stream6);

  DMA_InitStructure.DMA_Channel = DMA_Channel_2;  

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) &(TIM4->CCR1);

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) TIM4_CCR1_SRC;

  DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToPeripheral;

  DMA_InitStructure.DMA_BufferSize = DMA1_TIM4_Pulse;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;         

  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init(DMA1_Stream6, &DMA_InitStructure);

  

  /* TIM4_CCR1 DMA1_Stream6 Channel 2 */

  DMA_ITConfig(DMA1_Stream6, DMA_IT_TC, ENABLE);

  NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  

  NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream6_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  /* Time base configuration */

  TIM_TimeBaseStructure.TIM_Period = uhTimerPeriod;

  TIM_TimeBaseStructure.TIM_Prescaler = 0;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);

  TIM4->CNT = 0;

 

  /* PWM1 Mode configuration: Channel1 */

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

  TIM_OCInitStructure.TIM_Pulse = TIM4_CCR1_SRC[0];

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

  TIM_OC1Init(TIM4, &TIM_OCInitStructure);

  TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);

  TIM_ARRPreloadConfig(TIM4, ENABLE);

//  TIM_Cmd(TIM4, ENABLE);

  TIM_GenerateEvent(TIM4, TIM_EventSource_Update);

  /* TIM4 Update DMA Request enable */

  TIM_DMACmd(TIM4, TIM_DMA_Update, ENABLE);

  

  TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE);

}

void main(){

  ..

  TIM4_PWM_DMA_Config();

  while(1){

    // for send 10 Pulse

    TIM4->CNT = 0;

    TIM4->CR1 &= ~TIM_CR1_OPM;

    TIM4->CR1 |= TIM_CR1_CEN;

    DMA1_Stream2->NDTR = DMA1_TIM4_Pulse_Number;

    DMA_Cmd(DMA1_Stream2, ENABLE);

  }

}

/**

  * @brief  This function handles DMA1_Stream4 global interrupt request.

  * @param  None

  * @retval None

  */

/**

  * @brief  This function handles DMA1_Stream0 global interrupt request.

  * @param  None

  * @retval None

  */

void DMA1_Stream6_IRQHandler(void)

{

  if (DMA_GetITStatus(DMA1_Stream6, DMA_IT_TCIF6) != RESET) {

    DMA_Cmd(DMA1_Stream6, DISABLE);

    DMA_ClearITPendingBit(DMA1_Stream6, DMA_IT_TCIF6);

    TIM4->CR1 |= TIM_CR1_OPM; // End PWM

  }

}

#tim4_ch1_pwm_dma-stm32cubemx
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
chrif
Associate II
Posted on June 23, 2015 at 17:05

Hi,

you van refer to the User manual UM1718 under Help->About of the CubeMx interface or under the link

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00104712.pdf