cancel
Showing results for 
Search instead for 
Did you mean: 

High speed op optocoupler with non-inverted op.

parth kothiya
Senior

i am using 6N137 high speed optocoupler but problem is op is inverted.

so i required high speed (frq >= 100KHz) optocoupler with non-inverted op.

or how can i get non inverted op using 6N137 ?

0693W00000AMiduQAD.jpg

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Just change the drive circuit:

  • via software: invert the logical level at PB9, e.g. by programming of the driving mcu
  • via hardware: connect pin 3 to primary GND and drive the optocoupler at pin 2, alternatively invert the signal using a transistor with pull-up at the input or output of the optocoupler

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.