cancel
Showing results for 
Search instead for 
Did you mean: 

help with ft232rl and discoveryf4

montagnanigiovanni
Associate II
Posted on August 28, 2014 at 14:04

hi everybody, i need to interface my dicovery board with a ft232rl board that i bought from amazon.

i'm running this program i wrote:

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart1;

/* USER CODE BEGIN 0 */

void ERROR_HANDLER();

/* USER CODE END 0 */

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_USART1_UART_Init(void);

int main(void)

{

  /* USER CODE BEGIN 1 */

char data2send='g';

    

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  /* System interrupt init*/

  /* Sets the priority grouping field */

  HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);

  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_USART1_UART_Init();

  /* USER CODE BEGIN 2 */

  HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,1);

    HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,1);

  /* USER CODE END 2 */

  /* USER CODE BEGIN 3 */

  /* Infinite loop */

  while (1)

  {

  if(HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_0)==1)

    {

        HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,0);

      HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,0);

        HAL_UART_Transmit(&huart1,(uint8_t*)data2send,1,200);

        HAL_Delay(300);

        HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,1);

      HAL_GPIO_WritePin(GPIOD,GPIO_PIN_12,1);

        if(HAL_UART_Transmit(&huart1,(uint8_t*)data2send,1,200)!= HAL_OK)

        {

            ERROR_HANDLER();

        };

        

    }

  }

  /* USER CODE END 3 */

}

/** System Clock Configuration

*/

void SystemClock_Config(void)

{

  RCC_ClkInitTypeDef RCC_ClkInitStruct;

  RCC_OscInitTypeDef RCC_OscInitStruct;

  __PWR_CLK_ENABLE();

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

  RCC_OscInitStruct.HSEState = RCC_HSE_ON;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

  RCC_OscInitStruct.PLL.PLLM = 8;

  RCC_OscInitStruct.PLL.PLLN = 336;

  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

  RCC_OscInitStruct.PLL.PLLQ = 7;

  HAL_RCC_OscConfig(&RCC_OscInitStruct);

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1

                              |RCC_CLOCKTYPE_PCLK2;

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

  HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);

}

/* USART1 init function */

void MX_USART1_UART_Init(void)

{

  huart1.Instance = USART1;

  huart1.Init.BaudRate = 110;

  huart1.Init.WordLength = UART_WORDLENGTH_9B;

  huart1.Init.StopBits = UART_STOPBITS_1;

  huart1.Init.Parity = UART_PARITY_ODD;

  huart1.Init.Mode = UART_MODE_TX;

  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart1.Init.OverSampling = UART_OVERSAMPLING_16;

  HAL_UART_Init(&huart1);

}

/** Configure pins as

        * Analog

        * Input

        * Output

        * EVENT_OUT

        * EXTI

*/

void MX_GPIO_Init(void)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  /* GPIO Ports Clock Enable */

  __GPIOH_CLK_ENABLE();

  __GPIOA_CLK_ENABLE();

  __GPIOD_CLK_ENABLE();

  /*Configure GPIO pin : PA0 */

  GPIO_InitStruct.Pin = GPIO_PIN_0;

  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /*Configure GPIO pins : PD12 PD13 PD14 */

  GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14;

  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

}

/* USER CODE BEGIN 4 */

void ERROR_HANDLER()

{

    while(1)

    {

    HAL_Delay(50);

        HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_14);

      HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_12);

    }

}

and i correctly see the tx led blinking two times every time i push my blue button.

why i receive with real term only zeros?

do you think is a hardware problem?

thank you so much for your help

Giovanni
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
montagnanigiovanni
Associate II
Posted on August 29, 2014 at 15:21

hi, i've changed usart (now i'm using usart6), now i see some bits arriving in real term.

they are not what i would like to send, but better something than nothing!

may someone help me founding what i did wrong?

it is because i'm using the uart library instead of the usart one?

it is correct how cubemx has set my port?

void MX_USART6_UART_Init(void)

{

  huart6.Instance = USART6;

  huart6.Init.BaudRate = 115200;

  huart6.Init.WordLength = UART_WORDLENGTH_8B;

  huart6.Init.StopBits = UART_STOPBITS_1;

  huart6.Init.Parity = UART_PARITY_NONE;

  huart6.Init.Mode = UART_MODE_TX_RX;

  huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart6.Init.OverSampling = UART_OVERSAMPLING_16;

  HAL_UART_Init(&huart6);

and how i use the library?

HAL_UART_Transmit(&huart6,(uint8_t*)data2send,1,200);

thank you.

Giovanni