2009-05-08 1:26 AM
Hardware CRC on byte buffer
2011-05-17 3:36 AM
The hardware CRC works on 4 bytes at a time (CRC->DR is a 32 bit register).
How do you CRC a buffer that contains a number of bytes not divisible by 4 i.e. what do you do with the last 1, 2 or 3 bytes? E.g. unsigned char buffer[5] = { 1, 2, 3, 4, 5 }; // CRC ???? Regards Trevor2011-05-17 3:36 AM
I am wondering if once again the documentaion is wrong and that
CRC_DR = CRC_DR + CRC_IDR (32bit) = (32bit) + (8bit) (where + means crc) might be worth a try. 8-) Otherwise whats the point of the CRC_IDR register?2011-05-17 3:36 AM
Hi bobz,
I wondered that also. Anyway I'm not going to use the hardware CRC now as it uses the wrong polynomial -- 0x4C11DB7 and I want to use 0xEDB88320. It's a shame you cannot set the polynomial. The reason I looked at hardware CRC was to reduce the size of my booloader i.e. not have to store the 1k CRC table in code. I got round this by generating the the CRC table in RAM rather than defining it in code. Regards Trevor2011-05-17 3:36 AM
Dit you see that 0x4C11DB7 is the bit-revered version of 0xEDB88320?
The implementation is common on hardware designs (fi. FPGA) but from C-code it is not. You have to bit-reverse the data before you write to the CRC_DR register. The result of the CRC calculation should be bit-reversed and negated (^ 0xFFFFFFFF). See also about this subject. It seems that there is a design flaw about the CRC calculation unit. I think that CRC_IDR register originally was intended to calculate the CRC on a single byte but they could not get it right on the implementation. It would be nice if they fix it on new devices.