2017-09-29 9:13 AM
Hi all!
I have an STM32L0 using the HSI to clock at 6MHz, and a LSE for the RTC.
Devices goes to sleep (STOP mode) and wakes up just fine.
But if I activate the RTC Alarm A interrupt, while restoring clocks I get a HAL_ERROR in the HAL_RCC_OscConfig() function.
More precisely here:
/* Check if the PLL is used as system clock or not */
if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_SYSCLKSOURCE_STATUS_PLLCLK) {.....
}
else
{ return HAL_ERROR; }Any clues into this?
Thanks!!!2017-09-29 9:19 AM
Decode the RCC state before that, make sure the HSI is clocking, the PLL is locked and sourced correctly.
2017-10-03 4:06 AM
Thank you
Turvey.Clive.002
for the suggestions.I have gotten a little bit deeper and realized that the device is actually not going to sleep, and this happens sometimes every couple of minutes, or could be a couple of days. If the HAL_RCC_OscConfig() is calledwhen the device is awake then it fails and goes to the Error_Handler();. Of course, it shouldn't be called when the device is awake, but this would happen if the device fails to go to sleep.
I have the following function to go to sleep:
void enterStopMode(void){
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 9, RTC_WAKEUPCLOCK_CK_SPRE_16BITS) != HAL_OK) {
TRACE_DBG_H('HAL ERROR -> HAL_RTCEx_SetWakeUpTimer_IT\n'); } HAL_CRC_DeInit(&hcrc); HAL_I2C_DeInit(&hi2c1); HAL_I2C_DeInit(&hi2c2); HAL_I2C_DeInit(&hi2c3); isSleep=true; TRACE_DBG_H('STOP\n'); HAL_UART_DeInit(&hlpuart1); __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI); HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);}
Sometimes this function doesn't go to sleep at all and code continues execution, where the HAL_RCC_OscConfig() is called and it fails as expected.
I noticed that in the Reference Manual (
) page 161, Table 37, it says:Note: To enter the Stop mode, all EXTI Line pending bits (in Section 5.6: EXTI pending register (EXTI_PR)), all peripherals interrupt pending bits, the RTC Alarm (Alarm A and Alarm B), RTC wakeup, RTC tamper, and RTC time-stamp flags, must be reset. Otherwise, the Stop mode entry procedure is ignored and program execution continues.
The only interrupt is the SysTick one. Could this be a race condition inside the
HAL_PWR_EnterSTOPMode that there's just an interrupt event before entering stop and makes it fail as per the note above?
void HAL_PWR_EnterSTOPMode(uint32_t Regulator, uint8_t STOPEntry)
{ uint32_t tmpreg = 0U;/* Check the parameters */
assert_param(IS_PWR_REGULATOR(Regulator)); assert_param(IS_PWR_STOP_ENTRY(STOPEntry));/* Select the regulator state in Stop mode ---------------------------------*/
tmpreg = PWR->CR; /* Clear PDDS and LPDS bits */ CLEAR_BIT(tmpreg, (PWR_CR_PDDS | PWR_CR_LPSDSR));/* Set LPSDSR bit according to PWR_Regulator value */
SET_BIT(tmpreg, Regulator);/* Store the new value */
PWR->CR = tmpreg;/* Set SLEEPDEEP bit of Cortex System Control Register */
SET_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk);/* Select Stop mode entry --------------------------------------------------*/
if(STOPEntry == PWR_STOPENTRY_WFI) { /* Request Wait For Interrupt */ __WFI(); } else { /* Request Wait For Event */ __SEV(); __WFE(); __WFE(); } /* Reset SLEEPDEEP bit of Cortex System Control Register */ CLEAR_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk);}
I'm not entirely sure if this could be the case. Any opinions?
Thanks all for your input.
Andrés
2017-10-04 2:20 AM
Hi all!
Can anyone help me as to how to avoid this Stop mode entry ignored? I checked EXTI_PR and it is 0, but still Stop mode is ignored due to the Systick timer, I think.
Note: To enter the Stop mode, all EXTI Line pending bits (in Section 13.5.6: EXTI pending register (EXTI_PR)), all peripherals interrupt pending bits, the RTC Alarm (Alarm A and Alarm B), RTC wakeup, RTC tamper, and RTC time-stamp flags, must be reset. Otherwise, the Stop mode entry procedure is ignored and program execution continues.
Thanks in advance!
Andrés