2020-09-24 4:09 AM
I am using STM32L072
hence referring to reference manual RM0376
Page . 280 Table.53 suggests that priority can be from 0 till 38
but when try
HAL_NVIC_SetPriority(IRQn_Type IRQn, uint32_t PreemptPriority, uint32_t SubPriority)
as per help above that function i can set Preemptpriority only from 0-3 , subpriority is of no use for cortex m0+
if i put more than 3 ,it becomes 0
I am confused between reference manual and HAL
Which is correct ?
2020-09-24 6:00 AM
If you set the priority of all your interrupts to the same thing, the "priority" listed in the table is the order they'll fire in. These are built-in values which cannot be changed. It's just saying that if multiple interrupts are pending, and if they have the same priority level, the one with the lowest IRQ number will be executed first.
It could definitely be written better, or at least clarified.
2020-09-24 8:35 PM
"If you set the priority of all your interrupts to the same thing, the "priority" listed in the table is the order they'll fire in. "
Not the case cause i have already tried and uart and systicktimer stuck just because they have same priority.it only works if i change uart priority to a higher number .
2020-09-24 8:45 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.