cancel
Showing results for 
Search instead for 
Did you mean: 

Getting less data than expected

bsp0524
Associate II
Posted on September 05, 2012 at 02:24

Hello,

I am working on vision module using SMT32F4 and OV7670. It is custom built board and here is more information

http://www.negtronics.com/vision-module

The problem I am having right now is with DCMI/DMA transfer. I am getting less data than expected, basically 4 pixels less per line. Did anyone have this issue? I am not sure if the data that I did receive is correct.

Can any of you guys paste a working sample code? Maybe the issue is with the register setup of OV7670. There is no good data sheet and there seems to be too many undocumented registers. Does anyone have a working register setup for QVGA or QQVGA image capture?

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0