cancel
Showing results for 
Search instead for 
Did you mean: 

Gave 15V as ADC input by mistake

terence-b
Associate II
Posted on January 03, 2013 at 12:26

Hi

After giving 15V to PC3 (ADC3 channel 13), I'm unable to reprogram the flash. It says ''Flash loader program reported an error''. If there is a remedy, how can I go around this?

Have I permanently damaged the MCU?

Thanks in advance

Terence

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
frankmeyer9
Associate II
Posted on January 03, 2013 at 13:45

You could try the usual steps, such as mass erase in bootloader mode.

Perhaps the damage is restricted to GPIOC and/or the ADC.

But if you had a pin connected to a low-resistance 15V source, chances are high the part is blown.