2012-01-11 6:04 AM
Pb with FreeRTOS and USB
Hello,
We are working on the STM3220-G Evaluation Board. We are using IAR compiler [V6.2] and running a test application with FreeRTOS [7.0.2] and the STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0 The USB is used as Device, asVirtual Com Port. I've already a problem of compatibilty because of interrupt priorities (see discussion ''Pb with FreeRTOS and USB'')
Now, as soon as I create a new task on FreeRTOS, my application systematically crashes (HardFault_Handler) I am not sure that the USB Stack of ST is compatible with FreeRTOS because of the interrupts needed by the USB stack. Can someone help me? Regards