cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Loader Demostrator Flash option bit setting

chjchoi2
Associate
Posted on February 23, 2010 at 09:59

Flash Loader Demostrator Flash option bit setting

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
chikos332
Associate II
Posted on May 17, 2011 at 13:41

Hi,

Data1 and Data2 are freely used for any purpose (you can store any value you want in there).

STDBY means Standby mode, please refer to RM0008 at this

http://www.st.com/stonline/products/literature/rm/13902.pdf

section ''4.3.5 Standby mode''. This bit means, when set that the last reset was caused by entering StandBy mode. As well as nRST_STOP that means that the last reset was caused by entering Stop mode:

PM0042 @

http://www.st.com/stonline/products/literature/pm/13259.pdf

table 8.

''

Bit 18: nRST_STDBY

0: Reset generated when entering Standby mode.

1: No reset generated.

Bit 17: nRST_STOP

0: Reset generated when entering Stop mode

1: No reset generated

Bit 16: WDG_SW

0: Hardware watchdog

1: Software watchdog

''