cancel
Showing results for 
Search instead for 
Did you mean: 

External crystal for USB needed?

claudio
Associate II
Posted on September 29, 2015 at 04:37

Is the STM32 series capable of handling low speed USB without external crystal?

Best regards.
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on September 29, 2015 at 05:41

Which STM32 specifically? Most of them need a crystal to get remotely close to the required accuracy/stability needed for USB.

Some of the newer offerings have a trimmed HSI/MSI capable of generating a suitable 48 MHz reference, you should review the check-box items in the assorted press-releases and product pages.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
claudio
Associate II
Posted on September 29, 2015 at 07:53

Thank you for quick reply. Yes, now I see that ST does indeed explicitely feature some of the MCUs as working ''crystalless''. Good. Best regards

claudio
Associate II
Posted on September 29, 2015 at 08:07

One additional question. I'm planning to use it for a keyboard controller. Since STM32 MCUs come with bootloader, I don't really need a programmer, to get my firmware on it, right?

Posted on September 29, 2015 at 08:11

Most have a USB DFU programming scheme, though if you want any chance of developing and debugging on the platform you really need some form of SWD/JTAG pod.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
claudio
Associate II
Posted on September 29, 2015 at 08:26

I see. So it's better to include a SWD socket into the design, for whatnot may happen. Good. Thanks you, clive1

Posted on September 29, 2015 at 08:40

You can do it as test points, edge castellations, or whatever floats your boat. Systems without this connectivity in some form are real hard to trouble-shoot. I'd recommend SWDIO, SWCLK, SWO, NRST, GND as a minimum, and ideally also USART1_TX and USART1_RX (or equivalent as called out in the System Loader (ROM) specs)

If you have space, using standardized connections will also save to lot of time and messing around.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..