cancel
Showing results for 
Search instead for 
Did you mean: 

Error in using FWLib 2.0.3 with Keil (Eval) version

hnaqvi
Associate II
Posted on November 11, 2008 at 05:38

Error in using FWLib 2.0.3 with Keil (Eval) version

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
hnaqvi
Associate II
Posted on May 17, 2011 at 12:51

Hi!

I just updated with the new version of FWLib 2.0.3 for Cortex M3. I just made a new project with the help of template given in the library for RTC Calender example. The project compiles fine. I turned the debug option from ULINK to Simulator and when I tried to simulate the code I got an error. Plz see attached images. I would be grateful if some one could help me :(

Cheers,

-Hassan

16-32micros
Associate III
Posted on May 17, 2011 at 12:51

Hi Hassan,

I believe that only the projects inside Keil Installation folder :

''C:\Keil\ARM\Boards\Keil\MCBSTM32 ''are supporting simulation features with µVision.

Else you need a hardware board and a real silicon with Ulink to run the examples on real STM32 micro.

Regards,

STOne-32.

hnaqvi
Associate II
Posted on May 17, 2011 at 12:51

I see! Yes probably this is the problem! Many thanks for the prompt reply.

Regards,

-Hassan