cancel
Showing results for 
Search instead for 
Did you mean: 

Endpoint problem.

tonykwon
Associate
Posted on October 30, 2011 at 08:01

Hello,

I have STM3210C-EVAL board. The HID mouse example is working well.

But, if I change the endpoint from 0x81 to 0x82, it doesn't work.

In addition, for TX2 buffer I changed buffer size to 128 like

#define TX2_FIFO_FS_SIZE 128.

Andybody with this kinds of problem?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
eliahuroash
Associate
Posted on October 22, 2013 at 09:38

can answer me if you resolve the problem ?

how you resolve the problem?

Posted on October 22, 2013 at 14:11

A single post from two years ago, probably not.

Please state clearly your situation and perhaps you can get an answer about that.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jzawadzk
Associate II
Posted on October 22, 2013 at 19:01

My guess is that you should increase by one value of

#define EP_NUM

located in usb_conf.h