cancel
Showing results for 
Search instead for 
Did you mean: 

Encoder Mode

stuart2399
Associate II
Posted on February 18, 2008 at 09:45

Encoder Mode

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stuart2399
Associate II
Posted on May 17, 2011 at 12:23

Hi STOne-32 / All.

I wish to use the Encoder Mode (a sub mode of the TIMers). This uses two signals in quadrature to count from an incremental encoder.

--------------------------------------------------------------------------

Q1 : Is there any example code for this mode?

--------------------------------------------------------------------------

Q2 : Is it possible to cascade two timers in encoder mode - to get 32 bit counting? (I'm guessing not because you'd need two trigger out lines from the master and two trigger in lines for the slave. There only seems to be 1 trigger available).

Note: I've read the post about ''Cascading timers overflow handling and capture'' by andywild (Posted 20-01-2008 at 12:29) and AN2592 in detail.

--------------------------------------------------------------------------

Q3 : To Use Encoder Mode, do I have to use TIMx_CH1 & TIMx_CH2 pins (or can I use any e.g. TIMx_CH3 & TIMx_CH4)

--------------------------------------------------------------------------

Please could you give me some advice!

Thanks.

stuart2399
Associate II
Posted on May 17, 2011 at 12:23

Hi All,

Any ideas on using the Timers in Encoder Mode (as per my first query)?

Thanx