cancel
Showing results for 
Search instead for 
Did you mean: 

EmCraft supports the smt32f429i-disco with networking

magore
Associate II
Posted on February 11, 2014 at 04:34

Just a few days ago i noticed that EmCraft released supports for the smt32f429i-disco with networking (with board modifications needed and and external PHY)

I have just tested this code on my board

Note: it requires an external PHY DP83848 (available on Ebay) this can be wire-wrapped to the board

Here is my console log

U-Boot 2010.03-linux-cortexm-1.12.1 (Jan 21 2014 - 10:22:44)

CPU  : STM32F4 (Cortex-M4)

Freqs: SYSCLK=180MHz,HCLK=180MHz,PCLK1=45MHz,PCLK2=90MHz

Board: STM32F429-DISCOVERY Rev 1.A

DRAM:   8 MB

In:    serial

Out:   serial

Err:   serial

Net:   STM32_MAC

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 08040000 ...

   Image Name:   Linux-2.6.33-arm1

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    1668000 Bytes =  1.6 MB

   Load Address: d0008000

   Entry Point:  d0008001

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Linux version 2.6.33-arm1 (root@media) (gcc version 4.4.1 (Sourcery G++ Lite 204

CPU: ARMv7-M Processor [410fc241] revision 1 (ARMv7M)

CPU: NO data cache, NO instruction cache

Machine: STMicro STM32

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 2032

Kernel command line: stm32_platform=stm-disco console=ttyS0,115200 panic=10 ip=5

PID hash table entries: 32 (order: -5, 128 bytes)

Dentry cache hash table entries: 1024 (order: 0, 4096 bytes)

Inode-cache hash table entries: 1024 (order: 0, 4096 bytes)

Memory: 8MB = 8MB total

Memory: 6420k/6420k available, 1772k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0x00000000 - 0x00001000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0x00000000 - 0xffffffff   (4095 MB)

    lowmem  : 0xd0000000 - 0xd0800000   (   8 MB)

    modules : 0xd0000000 - 0xd0800000   (   8 MB)

      .init : 0xd0008000 - 0xd0092000   ( 552 kB)

      .text : 0xd0092000 - 0xd018f000   (1012 kB)

      .data : 0xd0190000 - 0xd019f3a0   (  61 kB)

Hierarchical RCU implementation.

NR_IRQS:90

Calibrating delay loop... 36.45 BogoMIPS (lpj=182272)

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Switching to clocksource cm3-systick

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 512 (order: 0, 4096 bytes)

TCP bind hash table entries: 512 (order: -1, 2048 bytes)

TCP: Hash tables configured (established 512 bind 512)

TCP reno registered

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Serial: STM32 USART driver

stm32serial.0: ttyS0 at MMIO 0x40011000 (irq = 37) is a STM32 USART Port

console [ttyS0] enabled

blackfin-eth: found MAC at 0x40028000, irq 61

blackfin_mii_bus: probed

found PHY id 0x20005c90 addr 1

eth0: using MII interface

eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=00:01, irq=-1)

TCP cubic registered

NET: Registered protocol family 17

ARMv7-M VFP Extension supported

IP-Config: Guessing netmask 255.255.255.0

IP-Config: Complete:

     device=eth0, addr=192.168.200.111, mask=255.255.255.0, gw=255.255.255.255,

     host=stm-disco, domain=, nis-domain=(none),

     bootserver=192.168.200.240, rootserver=192.168.200.240, rootpath=

PHY: 00:01 - Link is Up - 100/Full

Freeing init memory: 552K

~ #

~ # nslookup time.nrc.ca 192.168.200.240

Server:    192.168.200.240

Address 1: 192.168.200.240 240.200.168.192.in-addr.arpa

Name:      time.nrc.ca

Address 1: 132.246.11.228 time.nrc.55.11.246.132.in-addr.arpa

Address 2: 132.246.11.227 time.nrc.55.11.246.132.in-addr.arpa

Address 3: 132.246.11.229 time.nrc.55.11.246.132.in-addr.arpa

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0