2014-02-24 7:42 AM
2014-02-28 3:43 AM
Thanks Francescato Diego and Clive1 for the suggestions,
@ Francescato Diego you wrote ''only trigger SDIO DMA transfer when you have a block of 512 bytes ready
''. Did you mean that data should only be tranfer data by only this function ''SD_LowLevel_DMA_TxConfig(uint32_t *BufferSRC, uint32_t BufferSize)'' and then disabling the SDIO stream. or should I just use following functions and then disable streamDMA_FlowControllerConfig(SD_SDIO_DMA_STREAM,DMA_FlowCtrl_Peripheral);/* DMA2 SDIO stream enable */DMA_Cmd(SD_SDIO_DMA_STREAM, ENABLE);Thanks in advance...2014-02-28 6:26 AM
I wrote
my
SDIO
driver
(
is
a first version
and
I have some problems
, but it works)I don't
use
the ST library
with SD card is in recv mode I writeconsecutive
blocks of 512bytes with this codecase SD_OP_WRITEBLOCK038:
SDIO_DMACmd (ENABLE); // I think is in a wrong position and this cause a DMA fifo error at transfer start (I read a recently appnote from ST)
SD_DMA_config (sd.data.ptr, (sd.data.blocks * SD_BLOCK_SIZE), DMA_DIR_MemoryToPeripheral) ;
SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT;
SDIO_DataInitStructure.SDIO_DataLength = (uint32_t) (sd.data.blocks * SD_BLOCK_SIZE);
SDIO_DataInitStructure.SDIO_DataBlockSize = (uint32_t) SD_BLOCK_SIZE_2POWER;
SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard;
SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;
SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;
SDIO_DataConfig(&SDIO_DataInitStructure);
sd.opstate = SD_OP_WRITEBLOCK045;
case SD_OP_WRITEBLOCK045:
if (sd.DMAtransfer) break ;
if (!(SDIO->STA & SDIO_FLAG_DATAEND)) break ;
if (SDIO->STA & SDIO_FLAG_TXACT) break ;
SD_disable_data_path () ;
My SD_DMA_config is similar to SD_LowLevel_DMA_Tx config DMA for data transfer
after this call I see with emulator the DMA stream fifo is loaded with first 4 dword data and wait the SDIO data path enable before write to SDIO fifo
(Frank blog explain very well the transfer mechanism)
The sd.DMAtransfer is a flag set to 1 (in SD_DMA_config) while DMA transfer in progress and reset in DMA interrupt procedure when trasfer is complete
Note that the DMA fill SDIO fifo and when DMA transfer is complete the SDIO transmission is still in progress
Before disable data path you must wait SDIO end of transmission. In this driver release I have added two bit test but this check is work in progress.
I also tried the solution that you suggest with the fewest number of possible configurations for DMA but did not work for me and I have not investigated
static void SD_DMA_enable (uint32_t p, uint32_t len, bool dir)
{
sd.DMAerror = 0 ;
sd.DMAtransfer = 1 ;
DMA_Cmd (SD_DMA_STREAM, DISABLE);
DMA_MemoryTargetConfig (SD_DMA_STREAM, p, DMA_Memory_0) ;
DMA_SetCurrDataCounter (SD_DMA_STREAM, len/4) ;
DMA_SelectDirection (SD_DMA_STREAM, dir) ;
DMA_StreamEventFlagClear (SD_DMA_STREAM, DMA_IT_FLAGS) ;
DMA_Cmd (SD_DMA_STREAM, ENABLE);
}
2014-02-28 9:17 PM
Thanks Francescato Diego for the code example. Can you put your SDIO driver here, It may be helpful to alots of people working with SDIO.
2014-03-02 3:59 AM
uhm ...
my boss
fire me
... he
pays me
for
the firmware development.
The driver is not difficult to create require only few days starting from zero (like me)With Google
you can find
several
examples .
ask me
all you need
and
I'll help you
(
withmy bad english
...
)In my opinion
for this application
you just have to
break the
SDwrite
procedure from ST libraryinto three
procedures
:The
firstcalled
before start acquiring
formDCMI
puts
the SDcard
in
recv
mode (ST library SD_WriteMultiBlocks
but without the last call SDIO_DataConfig )The second
that
triggers
the
DMA
after rx
512 bytes block
, (New procedure with DMA config and call to SDIO_DataConfig) The third that
sends
thestop command to card after
acquisition
completed
(ST library SD_StopTransfer())
2014-03-02 11:07 PM
No issue, in your last post what does this function mean
SD_disable_data_path () ;
does it mean disabling the straem or DMA or both?I set the sd card to receive mode and I found some success (thanks for the suggestion)...2014-03-03 3:05 AM
static void SD_disable_data_path ()
{
SDIO->DCTRL &= ~SDIO_DPSM_Enable ;
} DMA stop is automatic mode after block transfer
2014-03-07 1:38 AM
@Francescato I have putted the SD card in receive (multiple block) mode but it still seems to be writing a few blocks. I have also tried the SDIO with polling mode but the problem still remains the same (few blocks written).
@Clive1 Here are some of the parameters of my dataPixel clock = 27MHzHsync = 15.6KHzCamera Ressolution = 720*480 (25 fps)Pixel Format YCbCr 4:2:2SDIO clock 24MHzSDIO class = 42014-03-07 7:17 AM
Ok, but that really doesn't suggest you've worked through the math here.
What is the WRITE bandwidth of you SD/SDHC card? Can you demonstrate that OUTSIDE of your streaming from the camera concept. Test your code and understand it's functionality and performance, and do this independently of anything else using data patterns you control and understand. Verify that it writes properly, and quantify how quickly it does so. Somehow the card spec would suggest a write speed below 6 MBps, and perhaps as bad as 2 MBps. You video spec suggests you're generating frame data in the order of about 9 MBps, and arguably getting bursts in the order of 27 MBps How do you plan on handling these disparities?2014-03-07 8:23 AM
Follow the Clive suggestions
I
just add
some
technical info:
You mustread
the
cardCSD
register
during the
driver init procedure This register contain info about the
maximum write speed for card.
With this info you canconfigure
the SDIO clock PLL
and you must
use
class 10
devices
for
high-speed
write
Before start write
new data block check for driver errors
and first query the state of the card withCMD13
The CMD13 reply contain the card status if card busy you must wait previous write end before write next block (card status recv)(
SD
specs.explain in detail
the change of state
when accessing
the SD card
...I
can't explain it
clearly
with my bad english)2014-03-07 11:47 PM
thought night ...
Frank in his blog
http://blog.frankvh.com/2011/12/30/stm32f2xx-stm32f4xx-sdio-interface-part-2/ answers a question asVery useful , Explained in great detail .
Thanks a lot!
Out of curiosity : Did you try to operate the SD interface at 25MHz than blackberries ?
48MHz Should Be possible?
What was the best write speed Could you manage ?
Frank 's answer
I've personally not run faster than 20 MHz , two to the repute my hardware Has a level converter ( 1.8V - 3.3V ) between the STM32 and the SD Card Given That, the fastest write speed 've Has Been Achieved
9 MB / s Which actually is not too bad (I'll admit it , I was happy ) .
I've no doubt faster speeds are possible , but you'd certainly need to run the STM32 at 3.3V so you can avoid a level converter to make SD Card Those faster clock speeds possible.
I think if you
write
a driver
SD
taking care of the
details and
using the right
SD card
you should
get this
result.
But you have a problem because your DCMI and SDIO peripherals share the same DMA .
I never used the DCMI peripheral butI have read
the datasheet
:If you transfer
8 bits / pixel
at 27MHz
I read
that
DCMI
trigger
an interrupt when
a
dword
is ready
then
the
DMA
interrupt
frequency
is
around
7MHz
(
...
right
?)
I've read that DCMI can exec hw JPEG compression does not know how it works and how it change the the bit rate, but you could try ( if you do not already ) An alternative (also in this case to be studied the transfer time) would be connect an NAND flash on the FSMC bus (which device you uses ? ) The peripheral do ECC in hardware and you will have deal ''only'' with wear levelingIn this way the
DCMI
could transfer
in
DMA
directly
in the flash memory
.