cancel
Showing results for 
Search instead for 
Did you mean: 

DMA Hangs When Sys Clock Lowered

jvavra
Associate III
Posted on September 11, 2014 at 14:18

I use three DMA channels to transfer data via SPIs on a STM32F427VG. I normally run SYSCLK at 168MHz, with SPIs prescaled down to 21MHz, and everything works fine. I'm working on tracking down a noise issue, so I am trying to reduce clock speeds. I used the Clock Configurator tool to generate a new system_stm32f4xx.c file to run at 96MHz (SPIs dropped to 12MHz). 

However, this seems to cause one of the DMA channels to hang; I'm having trouble pinpointing how long but it seems to take multiple mS after transmitting for one of the DMA streams to become available again.

Any thoughts?

 

#stm32-dma
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0