cancel
Showing results for 
Search instead for 
Did you mean: 

DMA desc. in Ref. Manual STM32F4: Possible misprint/error?

flyer31
Senior
Posted on January 31, 2012 at 21:46

In Ref Manual DMA configuration, many register bits have the condition: ''can be written only if EN=0''. This is ok from my side.

But the last two bits in the list, FTH (Fifo Threshold), have the condition: ''can be written only if EN=1''. I think this is a misprint? (At least the StdPeriphLib-File stm32f4xx_dma.c writes them when EN=0 - so either manual wrong or procedure in stm32f4xx_dma.c wrong).
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0