cancel
Showing results for 
Search instead for 
Did you mean: 

Disable HSI RC when using PLL-HSE as system clock

michaellange9
Associate II
Posted on July 15, 2008 at 12:21

Disable HSI RC when using PLL-HSE as system clock

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
michaellange9
Associate II
Posted on May 17, 2011 at 12:39

Hey gays,

I'm using the STM3210B-Eval board with IAR EWB and writing my own firmware for better understanding the micro...

When I configure the PLL circuit driven by the 8MHz external oszillator (HSE is choosen), can't I turn off the HSI RC part by writing Bit HSION in Register RCC_CR to 0? I'm doing that at the end, when all other clock configurations are done.

My debugger runs to memory ''0xFFFFFFFF UNDEFINED INSTRUCTION''...

Cheers,

Michael

michaellange9
Associate II
Posted on May 17, 2011 at 12:39

Ok...solved by setting the correct Flash Latency... (RM0008 page 40)