cancel
Showing results for 
Search instead for 
Did you mean: 

DFU for STM32103x

slaven
Associate
Posted on February 02, 2009 at 18:22

DFU for STM32103x

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slaven
Associate
Posted on May 17, 2011 at 13:01

Hi,

I have a Keil eval board MCBSTM32 (ver 5.1.1) and trying to incorporate DFU. I am able to enter the DFU mode (by using code from STMicro website and implementing necessary mods to the code). I can connect to my PC, recognize the USB devide, installed the driver the first time and able to enter DFU mode. I am also able to create a .DFU file for a simple project. However when I try to download app.dfu, the app gets stuck in erase mode. I get ''Target 00 upgrading - erase phase [22%]''.

I have made sure to change the starting vector address to 0x08003000 and the target and linker options to start the flash address at 0x08003000.

Appreciate any pointers!

Thanks,