Custom PWM Triggering in Center Aligned Mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-09-05 10:57 PM
Posted on September 06, 2014 at 07:57
I have looked at Dead Time insertion and got about a 2 degree change, unfortunately this is not enough. Other options I am looking at are Encoder Mode, I cant get any output in this more I am guessing because its looking for an external Trigger. I am also looking at Center Aligned mode. I am wanting to use Timer 8 Channel 1 and Channel 2 to be able to achieve this, is this possible using the same Timer? I am unfortunately a little lost and would appreciate some advice. Thank You. Chris P.S: Pin Inverting does not achieve what I need as the wave is not 180 degrees out of phase if Duty is adjusted. #phase-shifted-frequency-between
Hi, I am new to ST.
I have a STM32F405 MCU. Can someone please advise on the best way to customise PWM Output. I need to create a wave that is 180 degrees out of phase both with the same Frequency, Duty Cycle adjustable and also be adjustable for any necessary Frequency Changes.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-09-06 2:04 AM
Posted on September 06, 2014 at 11:04
Ok, I see it. Timer Synchronisation. My goal can be achieved by Syncronising two separate Timers, one Master, one Slave and setting them via the Manual:
See Pages: P. 606, P. 554 for info…// Configure Master Timer - Mine is Timer 8 Channel 1
CR2.SetBits(1 << 5); // <--- Bits 6:4 MMS[2:0]: Master mode selection
// Congifure Slave - My case is Timer 1 Channel 1
SMCR.SetBits(7 << 1); // <--- Bits 2:0 SMS: Slave mode selection
SMCR.ClearBits(7 << 4); // <--- Bits 6:4 TS: Trigger selection
Yes I am using the Microframework...
All the best
Chris