2016-05-01 8:49 AM
Hello ST team,
I like to see a critical section implementation similar to atmel avrlib ATOMIC_BLOCK implementation. example: ATOMIC_BLOCK(5) { uint8_t status get_spi_device_info(); if(status == 0) return; do_some_more_spi_communication(); } pls refer http://www.nongnu.org/avr-libc/user-manual/group__util__atomic.html and http://www.mikrocontroller.net/topic/312246#new basically: - the code should avoid blocking all interrupts - the code must allow to use break and return - the MCU status after the code must be the same as before the code squence - the code should higher the baseprio based on given argument - the code must not lower the baseprio if current cpuprio is higher than given baseprio use cases: - SPI device with notification signal main thead avoids to be interrupted by pin event handler - I2C devices communication from main thread and ISR - semaphore like operations ST there is obviously a need for this and many people are implementing self brewed implementation. Pls provide some proven code. Regards, Adib. --