cancel
Showing results for 
Search instead for 
Did you mean: 

CPAL code in open source projects

Posted on November 26, 2014 at 00:47

Can anyone confirm whether CPAL code can be used in open source projects.

I'm working on a port so that STM32F103 can be used with the Arduino 1.5.x environment.

I'd like to use some code from the CPAL library, For Example for hardware I2C, but I think this is not allowed under the CPAL license.

Can someone confirm if this is the case.

Thanks
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0