cancel
Showing results for 
Search instead for 
Did you mean: 

Conflicting of two interruptions configuration

aymane
Associate
Posted on June 13, 2014 at 15:51

Hello,

I have a problem to configure two interruptions in the same time. The first one is to receive data from UART, the second one is to send data to motors. After several successful itterations, UART Status stops at RESET, when the other routine continue to work. You find follow the configurations of the two interruptions :

/********************  Config IRQ TIM2 **********************/

void INTTIM_Config_cmd(void)

{

    TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

  NVIC_InitTypeDef NVIC_InitStructure;

  // Enable the TIM2 gloabal Interrupt

  NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 5;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  // TIM2 clock enable

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

 //  Time base configuration

  TIM_TimeBaseStructure.TIM_Period = 5000 - 1;  // 1 MHz down to 1 KHz (1 ms)

  TIM_TimeBaseStructure.TIM_Prescaler = 84 - 1; // 24 MHz Clock down to 1 MHz (adjust per your clock)

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

  // TIM IT enable

  TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

  // TIM2 enable counter

  TIM_Cmd(TIM2, ENABLE);

}

/********************  Config IRQ UART **********************/

void Wifi_HAL_uart_Init(uint32_t baudrate)

{

    GPIO_InitTypeDef GPIO_InitStructure;

    USART_InitTypeDef USART_InitStructure;

    NVIC_InitTypeDef NVIC_InitStructure;

    /* Enable GPIO clock */

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

    /* Enable UART clock */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART5, ENABLE);

    //RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

    /* Connect PXx to USARTx_Tx*/

    GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_UART5);

    /* Connect PXx to USARTx_Rx*/

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_UART5);

    /* Configure USART Tx as alternate function  */

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_Init(GPIOC, &GPIO_InitStructure);

    /* Configure USART Rx as alternate function  */

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);

    /* Enable the USART1 Interrupt */

    NVIC_InitStructure.NVIC_IRQChannel = UART5_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    /* USART configuration */

    USART_InitStructure.USART_BaudRate = baudrate;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    USART_Init(UART5, &USART_InitStructure);

    USART_ITConfig(UART5, USART_IT_RXNE, ENABLE);

    /* Enable USART */

    USART_Cmd(UART5, ENABLE);

}

// UART routine

void UART5_IRQHandler(void)

{

    if(USART_GetITStatus(UART5, USART_IT_RXNE) != RESET) {

          RxBuffer[RxBufferHead] = USART_ReceiveData(UART5);

        RxBufferHead = (RxBufferHead + 1) % RX_BUFFER_SIZE;

    }

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0