cancel
Showing results for 
Search instead for 
Did you mean: 

Conflict with two EEPROM

jonathannakache9
Associate II
Posted on July 06, 2012 at 10:02

Hi,

With a STM32, I have a problem

to select

either

EEPROM

(

M24LR64-R and M24M02-DR)

on the same bus

I2C

.

Here are the

''device

select

code

'':

For

M24LR64

-R:  1 0 1 0     X 1  1 X

In the order

:  1 0 1 0 = Device type identifier   X = E2   1 1 = E1 E0 ( chip enable)   X = RW

For

M24M02

-DR:

1 0 1

0   1

X

X

X

In the order

: 1 0 1 0 = Device type identifier   1 = E2 ( chip enable)   X X = A17 A16 (MSB address bits )    X = RW

The two

address bits

A17

and

A16

for

M24M02

-DR

can not be

used

because they would

pose

a conflict with the

R

-

M24LR64

there is

there a way

around the problem

?

Thank you for your

response

,

#pounds-head-on-desk
This discussion is locked. Please start a new topic to ask your question.
27 REPLIES 27
John F.
Senior
Posted on July 11, 2012 at 16:49

Your test device select codes have bit 0 low which is a write. The data sheet suggests,

In I2C products, the device does not respond (NoAck) when a programming operation is in

progress. Data polling thus consists in sending a Device Code in a loop mode and tracking

the EEPROM acknowledgement. It is recommended to poll the device with a Write

instruction.

I'm not sure that helps! I still recommend writing your own bit bashed I2C - the ST implementation is very awkward and unforgiving.

emalund
Associate III
Posted on July 11, 2012 at 16:57

this has been confusing because sometimes the reference is to the

M24LR64-R and sometimes to the M24M02-DR

anyhow I am sure you need to have A16and A17 the same when writing the address and switching to read, do you?

Erik
Posted on July 11, 2012 at 16:57

but A17 bit and A16 bit are selected in the device_selected so you have 4 devices on the bus? if not the above makes no sense

The single device contains 4 arrays of 64KB (ie 256KB or 2Mbit), which array is expressed in the address of the I2C device, not the offset expressed in the following two bytes.

It's hanging presumably because the I2C device isn't ACKing because it doesn't recognize the address presented on the bus.

Presenting some code might be instructive to see if there is an issue there.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jonathannakache9
Associate II
Posted on July 11, 2012 at 17:22

yes, it's the problem.. no ACK

the code:

void
config_i2c()
{
unsigned 
char
chip_select = 0xAC; 
// 1010 1100
int
i = 0;
char
tx1_buffer[] =
''test''
;
char
rx1_buffer[100];
bzero(rx1_buffer,100);
I2C_InitTypeDef I2C_InitStructure;
I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;
I2C_InitStructure.I2C_OwnAddress1 = chip_select;
I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
I2C_InitStructure.I2C_ClockSpeed = 100000;
I2C_Cmd(I2C1, ENABLE);
I2C_DeInit(I2C1);
printf
(
''strlen(tx1_buffer) = %d

''
, 
strlen
(tx1_buffer));
I2C_Init(I2C1, &I2C_InitStructure);
while
(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));
I2C_ITConfig(I2C1, I2C_IT_EVT | I2C_IT_BUF , ENABLE);
write_EEPROM(0x0, chip_select, tx1_buffer, 
strlen
(tx1_buffer));
Delay_ms(5);
read_EEPROM(0x0, chip_select + 1, rx1_buffer, 
strlen
(tx1_buffer));
printf
(
''donnees recues de l'eeprom: %s

''
, rx1_buffer);
}

void
write_EEPROM(uint16_t ReadAddr, unsigned 
char
chip_select, 
char
*ptx1_buffer, 
int
len_tx1_buffer)
{
int
i = 0;
I2C_GenerateSTART(I2C1, ENABLE);
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
/*!< Send EEPROM address for write */
I2C_Send7bitAddress(I2C1, chip_select , I2C_Direction_Transmitter);
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
I2C_SendData(I2C1, (uint8_t)((ReadAddr & 0xFF00) >> 8));
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
I2C_SendData(I2C1, (uint8_t)(ReadAddr & 0x00FF));
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
for
(i = 0 ; i < len_tx1_buffer ; i++)
{
I2C_SendData(I2C1,*ptx1_buffer);
ptx1_buffer ++;
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
}
I2C_GenerateSTOP(I2C1, ENABLE);
while
(I2C1->CR1 & I2C_CR1_STOP);
}

emalund
Associate III
Posted on July 11, 2012 at 18:55

anyhow I am sure you need to have A16and A17 the same when writing the address and switching to read, do you?

 

 

you do not show your read routine where the above is essential when you turn the bus.  Please post it

Erik

jonathannakache9
Associate II
Posted on July 12, 2012 at 09:07

because that is

when I

send

I2C_Send7bitAddress(I2C1, chip_select , I2C_Direction_Transmitter);

I have not received the ACK from the device

emalund
Associate III
Posted on July 12, 2012 at 19:23

Is the E2 pin on the chip tied to Vcc?

is the !WC pin on the chip tied to ground?

Erik

jonathannakache9
Associate II
Posted on July 16, 2012 at 09:40

yes...